Vishay Intertechnology’s SiC45x Family of microBUCK® Synchronous Buck Regulators Honored With 21IC 2021 Top 10 Power Product Award
Devices Offer Output Current to 40 A in Compact 5 mm x 7 mm Package for Increased Power Density and Transient Response

Products mentioned:
SiC450, SiC451, SiC453Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Sept. 24, 2021 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its Vishay Siliconix SiC45x family of microBUCK® synchronous buck regulators has been named by 21IC as a 2021 Top 10 Power Product Award winner. Offering output current ratings up to 40 A in the compact PowerPAK® 5 mm by 7 mm package, the devices were honored in recognition of their increased power density and transient response compared to previous-generation regulators.
Now in their nineteenth year, the Top 10 Power Product Awards have become the industry benchmark for innovative power products. Voted on by engineers and selected by 21 IC editors after intense review, the award-winning products were chosen based on their technological innovation, energy efficiency, ease of application development, and market response.
The high power density of the SiC45x devices is made possible by co-packaging high performance n-channel trench MOSFETs with a PWM controller in a compact package. The regulators offer low operating current in idle mode, enabling peak efficiency up to 98 % and reducing power losses. Intended to simplify the design of high-performance point of load (POL) converters, the integrated devices require minimal external components for configuration and loop compensation.
The SiC45x family regulators offer current ratings of 15 A, 25 A, and 40 A with input voltages from 4.5 V to 20 V. They are internally compensated over the entire VIN and VOUT range of operation. Highly configurable, the devices combine their wide input voltage range with an adjustable output voltage from 0.3 V to 12 V. The extremely versatile regulators are ideal for a wide range of applications, including POL converters in cloud computing, enterprise servers, and industrial computers, in addition to networking, telecom, and storage systems.
The Top 10 Power Product Awards was presented on Sept. 15 during a ceremony at the 2021 21IC Power Supply Technology Seminar in Beijing. Sherry Huo, Sr. Product Application Engineer (Power IC, Siliconix Division) of Vishay China accepted the award on Vishay’s behalf. The complete list of winners is available at https://huodong.21ic.com/top10power/winner-list.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
 https://www.facebook.com/VishayIntertechnology
###
The DNA of tech.™ is a trademark of Vishay Intertechnology.
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/