News » 2020 Releases » Vishay Intertechnology -30 V P-Channel MOSFET in PowerPAK® 1212‑8S ...

Vishay Intertechnology -30 V P-Channel MOSFET in PowerPAK® 1212‑8S Package Offers Industry-Low RDS(ON) to Increase Power Density, Save Energy in Portable Electronics

Device Offers Industry-Low RDS(ON) of 3.5 mΩ and FOM of 172 mΩ*nC in 10.89 mm2 Package

SiSS05DN

Products mentioned:

SiSS05DN
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
MALVERN, Pa. — Feb. 10, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new -30 V p-channel TrenchFET® Gen IV power MOSFET that offers industry-low on-resistance of 3.5 mΩ at 10 V in the 3.3 mm by 3.3 mm thermally enhanced PowerPAK® 1212-8S package, in addition to best in class on-resistance times gate charge — a critical figure of merit (FOM) for MOSFETs used in switching applications — of 172 mΩ*nC. Purpose-built to increase power density, the space-saving Vishay Siliconix SiSS05DN is 65 % smaller than devices with similar on-resistance in 6 mm by 5 mm packages.

The on-resistance of the MOSFET released today is 26 % lower than the previous-generation solution and 35 % lower than the next best product on the market, while its FOM is 15 % lower than the closest competing device. These industry-best values result in reduced conduction and switching losses to save energy and increase battery run times in portable electronics, while minimizing voltage drops across the power path to prevent false triggering. The device’s compact form factor is easier to fit into designs with limited PCB real estate.

With its industry-standard footprint size, the SiSS05DN provides a drop-in upgrade to existing parts in applications utilizing 5 V to 20 V input rails. The MOSFET is ideal for adapter and load switches; reverse polarity protection; and motor drive control in battery-powered devices, battery chargers, consumer electronics, computers, telecom equipment, and more.

The device is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.

Samples and production quantities of the SiSS05DN are available now, with lead times of 12 weeks subject to market conditions.  

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.

facebook https://www.facebook.com/VishayIntertechnology

###

PowerPAK and TrenchFET are registered trademarks of Siliconix incorporated
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
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.®


Contact Us |
Where to Buy
  • Find a Distributor
  • Find a Sales Representative
| Request Sample | Technical Support | Privacy Center | Do Not Sell or Share My Personal Information | Terms and Conditions | Information Security | Terms of Use |

CONNECT WITH US

Copyright ©2025 Vishay Intertechnology, Inc.

ECIA Member