LIFETIME CALCULATOR INSTRUCTIONS
How To Use
The lifetime calculator helps to assess if application conditions allow a specific aluminum electrolytic capacitor, e.g. one selected with the parametric search, to reach the target lifetime of the application. The lifetime calculator provides some flexibility to allow lifetime calculation for more complex application situations. Below are some examples to illustrate its use:
- Enter MAL215097514E3 as ordering code
- Enter 70 (kHz) in the right box as the frequency for I2
- Enter the target lifetime as 15 (years) and 1 as the number of parallel branches
- Define an operating condition, e.g. with the name "not operating", with 67% per year (16 h/day) at 30 °C and 0 A ripple current for I1 to I3
- Define an operating condition, e.g. with the name "operating", with 33% per year (8 h/day) at 50 °C and 2.5A ripple current for I2 and 0 A for I1 and I3
- Enter MAL210417471E3 as ordering code
- Enter 100 (Hz) in the frequency field (right box) for I1, 0.3 (kHz) in the frequency field for I2 and 7 (kHz) in the frequency field for I3
- Enter the target lifetime as 15 (year)
- Set the number of parallel branches to 2
- Define a first operating condition as "non-operating", enter 6760 (h) as operating time per year, 30 ( °C) as Tamb and 0 (A) for I1 to I3
- Define a second operating condition as "balanced", enter 1900 (h) as operating time per year, 70 (°C) as Tamb, 0 (A) for I1, 10 (A) for I2 and 20 (A) for I3
- Add a third operating condition as "un-balanced", enter 100 (h) as operating time per year, 70 (°C) as Tamb, 4 (A) for I1, 10 (A) for I2 and 20 (A) for I3
Background
A capacitor can be used to store electrical energy. When electrical energy is stored in the capacitor, current flows into the capacitor. When electrical energy is taken out, current flows out of the capacitor. The current flowing in and out of the capacitor is called "ripple current". If the pattern, with which the current flows in an out of the capacitor, repeats, the repetition rate of this pattern is the frequency of the ripple current.
An aluminum electrolytic capacitor is not an ideal capacitor:
- When it is used to store and release electrical energy, some of the electrical energy is lost in this process and is converted to heat. Due to the internal construction of an aluminum electrolytic capacitor, the energy loss is not always the same. The heat loss for a ripple current with low frequency (< 1 kHz) is higher than that for a ripple current with high frequency (> 1 kHz). To transport this heat to the outside world, the temperature of the aluminum electrolytic capacitor needs to be higher than its ambient temperature.
- It has a limited lifetime. Due to physical and chemical processes, its characteristics change over time until the application in which it is used, no longer functions correctly. At that point the capacitor has reached "end of life". The time before the capacitor reaches "end of life" depends on the application conditions, the most important one being its operating temperature.
The operating temperature of the aluminum electrolytic capacitor depends both on its ambient temperature and the temperature rise needed to transport away the heat losses caused by the ripple current. The purpose of the lifetime calculator tool is to assess if, based on the values for these parameters in the application, it is likely that a specific aluminum electrolytic capacitor can operate long enough before "end of life" is reached.
The lifetime multiplier graphs in the datasheets allow various types of calculations for a given part and application conditions (See Introduction, section "Calculation of Useful life..."). Due to the various factors involved, using the graphs can be time consuming. The lifetime calculator automates much of this calculation for the most common case, determine if a part can meet the target lifetime. To do this, the lifetime calculator uses a digitized version of the lifetime multiplier graphs.
To allow the lifetime calculation, the application conditions need to be translated to normalized conditions. This involves two steps:
1. What is the application ripple current?
As mentioned before, a ripple current of low frequency generates more heat than a ripple current of high frequency. To allow the calculation, the RMS values of the ripple current components in the application are translated to an RMS ripple current IA that generates the same amount of heat as the application current, but has the frequency at which the rated ripple current is specified, e.g. 100 Hz.
To do this, the application ripple current components are divided by the ripple current correction factor for that frequency. Ripple current correction values at common frequencies are shown in the datasheet. An RMS addition of the translated application currents components results in the total translated ripple current. This can be done if the frequency components of the application ripple current are not phase related.
Values for IA/IR > 1.5 indicate that the calculation is sensitive to cooling conditions. Dense packaging or hot components decrease expected lifetime, whilst forced airflow increases expected lifetime.
2. What is the expected life in the application?
To add up the time under the various application conditions, the time is translated to an equivalent number of hours at maximum ambient temperature conditions. To do this, the duration of each application condition is divided by the lifetime multiplier for the application condition. The result is the number of hours of the capacitor's lifetime "used up" by that application condition. If the sum of translated hours is less than the specified lifetime of the capacitor, the capacitor can meet the target lifetime. The expected lifetime in the application is calculated by multiplying the target lifetime with the ratio of specified lifetime and "used up" lifetime.
The heat loss for a ripple current with low frequency (< 1 kHz) is higher than that for a ripple current with high frequency (> 1 kHz). The frequency dependent ripple current multiplier compensates for this difference. To separate the various frequency components of the ripple current, an analog/digital filter can be used. In most applications, 3 (main) frequencies are sufficient to describe the components of the ripple current in the various operating conditions, e.g. 300 Hz from the rectified 3-phase mains, 100 Hz for the operating conditions when the 3-phase mains is not balanced and all components > 1 kHz, caused by the switching power electronics.
An FFT analysis of the ripple current, e.g. as caused by a bridge rectifier, might show many more frequencies, as the ripple current is not sinusoidal. It is a safe approximation to use only the lowest frequency in combination with its ripple current multiplier to calculate the application current IA. If it is possible to enter more than 3 frequencies, one might be tempted to enter the amplitudes of all frequency components found with the FFT. The RMS addition off all these components in combination with their ripple current multipliers will result in a too low value of the application current IA. This calculation is not correct when the phase relation between the frequency components is fixed, like it is for the main frequency and its harmonics.
Support
The lifetime calculator is not designed to handle all lifetime calculation situations for all parts in the Vishay portfolio. Currently it only covers the products from the Vishay BCcomponents range. If you have questions when using this tool, feel free to contact Vishay with your question.
Website related
The issue is website related, e.g. the user interface or help functions do not work as expected or the tool produces results that are not in line with the datasheet. Send a PDF file of your calculation with your question to: web.group@vishay.com
Technical
The issue is technical and you would like to have a product specialist from Vishay to contact you. Send a PDF file of your calculation with the additional questions to: aluminumcaps2@vishay.com
Further reading
Aluminum Electrolytic capacitors have a lot of special characteristics that are not "normal" for a capacitor. To provide a background to their construction and how this relates to all these characteristics, Vishay provides the following additional reading material: